- Home /
- Audio/Video /
- VGA Splitters/Extenders
VGA Splitters/Extenders
We offer VGA splitters and VGA extenders from brands such as L-com, Adder and Aten. A VGA splitter is a device that takes a single VGA signal and splits it into two or more VGA signals. This allows you to connect two or more monitors to a single computer or video source. VGA splitters are often used in classrooms, conference rooms, and other settings where multiple people need to view the same content on a screen.
Our VGA extenders are devices that extends the length of a VGA signal. This can be useful if you want to connect a computer or video source to a monitor that is located far away. VGA extenders typically use a combination of copper cables and fiber optic cables to transmit the signal over long distances.
The VGA splitters and VGA extenders that we offer are from reputable brands such as L-com, Adder and Aten.
Here are some of the factors to consider when choosing a VGA splitter or extender:
- The number of outputs: How many monitors do you need to connect?
- The resolution: What is the maximum resolution that you need to support?
- The length: How far do you need to extend the signal?
- The features: Do you need any special features, such as audio passthrough or HDCP support?
Here are some of the benefits of using VGA splitters and extenders:
- They allow you to connect multiple monitors to a single computer or video source.
- They can extend the length of a VGA signal, allowing you to connect a computer or video source to a monitor that is located far away.
If you are looking for a way to connect multiple monitors to a single computer or extend the length of a VGA signal, then a VGA splitter or extender is a viable option. L-com is well known for our low or no minimum order quantities and fast response times. Please contact our knowledgeable technical support and sales teams if you have questions about our VGA splitters and VGA extenders or other components. Order one or more VGA splitters and VGA extenders now to receive same business day shipping!