To our valued customers, please note that our offices and warehouses will be closed on the following date, Thursday, June 19th, in honor of the Juneteenth holiday.
 
 
L-com

L-com's fiber optic tools consist of all the products you need to terminate both Multimode and Single mode fiber optic cable assemblies. Products in this category include: fiber cleaners, scribes, cable strippers, cutting tools, safety glasses and Kevlar shears. We also offer many products for cleaning fiber connector end faces. Our Cleaners are used to remove dirt, oil, and debris from the end of a fiber optic cable before it is terminated. This ensures that the connection is made properly and that there is no loss of signal. The Strippers are used to remove the outer jacket and buffer coating from a fiber optic cable. This exposes the optical fiber, which can then be spliced or terminated. Our Kevlar shears are used to cut through the Kevlar strength member of a fiber optic cable. This is necessary to expose the optical fiber for termination. The Scribes are used to make a small mark on the end of a fiber optic cable. This mark helps to align the cable with the connector during termination. Glasses are worn to protect the eyes from the laser light used in some fiber optic termination tools.

In addition to these basic tools, L-com also offers a variety of other fiber optic tools for more specialized applications. These tools include fusion splicers, cleavers, and OTDRs. A fiber optic tool kit from L-com is a must-have for anyone who works with fiber optic cables. The right tools can make the job of terminating and splicing fiber optic cables much easier and more accurate. L-com's fiber optic tools are high-quality and affordable, making them a great choice for any fiber optic technician. Order your Fiber Optic Tools now to get same business day shipping!