To our valued customers, please note that our offices and warehouses will be closed on the following date, Thursday, June 19th, in honor of the Juneteenth holiday.
If you need to move a rack enclosure around the WRK Series Caster Base is the perfect option to install. With a 1300 lb capacity, this caster base allows you to easily roll the enclosure into place while only adding 3/4" to the overall height. Preinstalled heavy-duty 3" non-locking casters save you time completing your project early.