- Home /
- Audio/Video /
- DisplayPort Extenders
DisplayPort Extenders - AdderLink & Tripplite
L-com offers DisplayPort Extenders including both Adderlink DisplayPort Digital KVM Extender 2 and Tripplite DisplayPort A/V extenders.
The Adderlink DisplayPort Digital KVM Extender 2 is a KVM extender that allows you to extend the video, audio, and USB signals from two DisplayPort computers to a single monitor, keyboard, and mouse. It has a maximum extension distance of 150 meters for one 1920 x 1080 display, or 100 meters for dual 1920 x 1200 or one 2560 x 1600 display. It also supports HDCP 1.4, so you can use it to extend the video signal from a Blu-ray player or other HDCP-protected device.
The Tripplite DisplayPort A/V Extender is an A/V extender that allows you to extend the video and audio signals from a DisplayPort computer to a single monitor. It has a maximum extension distance of 100 meters. It does not support USB, so you will not be able to share USB devices between the two computers.
The main difference between the two devices is that the Adderlink DisplayPort Digital KVM Extender 2 supports KVM, while the Tripplite DisplayPort A/V Extender does not. If you need to share a keyboard, mouse, and USB devices between two computers, then the Adderlink DisplayPort Digital KVM Extender 2 is the better option. However, if you only need to extend the video signal from one computer to another, then the Tripplite DisplayPort A/V Extender is a more affordable option.
L-com is a well-known provider of high-quality DisplayPort extenders. We are accessible by phone, chat, and email. We are a global leader in wired and wireless connectivity products, providing solutions for many major industries, including electronics, medical, industrial automation, military, and telecommunications. We are well known for our low or no minimum order quantities and fast response times. Please contact our knowledgeable technical support and sales teams if you have questions about our DisplayPort extenders or other components. Order these DisplayPort extenders now to receive same business day shipping!