To our valued customers, please note that our offices and warehouses will be closed on the following date, Thursday, June 19th, in honor of the Juneteenth holiday.
 
 
L-com

Simplifying Factory Automation and Integration with TKD Cables

Automation is transforming the way factories operate. Whether it’s precision machining, robotic assembly, or automated food packaging, efficiency and reliability are paramount. At L-com, we understand that the backbone of any automation system lies in its connectivity—and we’re proud to now offer a new line of high-performance industrial cables from TKD Kabel, a renowned German manufacturer known for its durable, flexible, and motion-tolerant cable solutions. 

These six categories of TKD cables are engineered specifically for demanding, high-motion environments. They simplify factory integration and deliver dependable performance across a range of automation-heavy industries. 

Industries That Depend on Automation 

From the automotive sector to logistics and food processing, automation has become indispensable for maintaining productivity, consistency, and safety. 

  • Cutting and grinding machinery rely on automation to perform precise, repetitive tasks at high speeds with minimal error. 

  • Lifting equipment and conveyors use sensors and motor controls to move parts and materials across large facilities. 

  • Material handling systems automate the transport of components and products, reducing the need for manual labor. 

  • Food processing and packaging applications demand sanitary, high-speed operation with extremely tight process control, often under harsh environmental conditions such as washdowns or extreme temperatures. 

Each of these applications places immense stress on cable infrastructure. From repetitive bending to electromagnetic interference, the wrong cable can mean costly downtime or safety hazards. That’s why TKD cables are built with specialized materials and designs to endure these tough operating conditions. 

Six Cable Categories Powering Modern Automation 

These cables are essential for transmitting control signals to motors, sensors, relays, and actuators across automated systems. TKD’s flexible control cables are designed to withstand continuous movement, tight bending radii, and repetitive flexing without fatigue. 

In robotics, for example, these cables power the motion of robot arms or end effectors while ensuring accurate feedback from sensors. In cutting and grinding machines, they handle both signal and low-voltage power in equipment that operates continuously, often around the clock. 

Tray cables are ideal for distributing control and power signals throughout industrial facilities via cable trays, ducts, or conduits. They’re often used in stationary or semi-stationary applications where mechanical protection and simplified routing are necessary. 

Manufacturers rely on tray cables to connect control panels, motors, and automated machinery. In material handling or packaging lines, these cables deliver consistent performance over long runs, often exposed to vibration or fluctuating temperatures. TKD tray cables offer resistance to oil, moisture, and chemicals, making them ideal for harsh environments. 

3. Bus Cables 

Automation systems depend on communication between machines, sensors, and controllers. TKD’s bus cables—including AS-i Bus, CAN Bus, and Profibus—are engineered to transmit data reliably in noisy industrial environments. 

In factory settings, bus cables are often used in distributed control systems where various components must coordinate in real time. For example, in automated bottling plants or CNC machining centers, bus cables enable synchronized operation between control units and individual machines. Their shielded construction minimizes interference and supports stable, high-speed communication. 

Servo and variable frequency drive (VFD) systems require specialized cabling to handle high voltages, switching frequencies, and EMI (electromagnetic interference). TKD’s servo and VFD cables are built to deliver clean, reliable power to motors and drives—even in high-speed, high-torque environments. 

These cables are indispensable in conveyor systems, robotic lifters, and precision tools that demand responsive control and fast acceleration. Their reinforced insulation and shielding help protect sensitive electronics from electrical noise, a common issue with VFD applications. 

Profinet is one of the most widely used industrial Ethernet protocols for real-time communication between devices. TKD’s Profinet cables support fast, deterministic data exchange, essential for advanced automation applications. 

These cables are critical in smart factories where process control, diagnostics, and system integration depend on seamless communication. Whether used in food processing automation or automotive assembly lines, TKD Profinet cables enable quick and reliable data transfer between PLCs, HMIs, and industrial sensors. 

Ethernet isn’t just for the office—it’s becoming increasingly central to industrial networks. TKD’s industrial-grade Category 5e, 6, and 6a Ethernet cables are ruggedized for use in harsh factory conditions, offering high-speed connectivity for everything from IP cameras to SCADA systems. 

These cables are built to endure mechanical stress, high humidity, and temperature swings, making them suitable for use in both control cabinets and field installations. In applications like automated warehousing, they keep systems online and communicating reliably even under constant vibration or motion. 

About L-com 

Ready to streamline your factory automation projects? Explore the wide selection of TKD cables now at L-com. We’ll fill your orders fast, with same-day shipping on all qualified, in stock, online orders received Monday through Friday before 5 p.m. EST. 

Resources

Search Entries